This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FlexNET Licensing Error (-96,491): "Server machine is down or not responding."



Hello,

Our lab has just acquired through TI's university program a CCsv5 with 100 users floating license, and I am having a hard time setting it up. I have followed all of the instructions in order to install the FlexNET server, and the service seems to be running just fine on our local server. I have also opened the 27000-27009 ports for the license manager so that other computers of our local network could connect to it.

However, whenever I try to connect to the server's license manager through Code Composer Studio 5, I would get an error message telling me that the "server machine is down or not responding" (error code -96,491). I've tried this with other computers in the lab, and the same error message always comes up. I've tried opening the same ports as the server (27000-27009) client side, it hasn't changed anything. I also tried to use the IP address of the server instead of its domain name, no luck either.

I've joined to this topic the logs that can be found on the FlexNET license manager, if it can be of any help. I'm at a loss here, did anybody have similar problems to the ones I am having ? Any tips on what I could investigate ?

Your help is greatly appreciated !

Louis

6443.access.log

2014-03-11 15:19:43,974 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-11 15:19:44,029 root.LicenseEngine started without redundancy.
2014-03-11 15:22:20,641 root.User User admin has changed their own password.
2014-03-11 15:23:11,213 root.Vendor (tidspssw) started.
2014-03-12 03:04:41,447 root.LicenseEngine stopped.
2014-03-12 03:09:12,122 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-12 03:09:12,793 root.LicenseEngine started without redundancy.
2014-03-12 03:09:15,928 root.Vendor (tidspssw) started.
2014-03-12 10:56:11,850 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-12 10:56:11,876 root.LicenseEngine started without redundancy.
2014-03-12 12:53:19,688 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-12 12:53:19,708 root.LicenseEngine started without redundancy.
2014-03-12 12:53:21,221 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-12 12:53:21,248 root.LicenseEngine started without redundancy.
2014-03-12 12:53:22,712 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-12 12:53:22,738 root.LicenseEngine started without redundancy.
2014-03-12 12:54:13,648 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-12 12:54:13,678 root.LicenseEngine started without redundancy.
2014-03-12 13:04:30,464 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-12 13:04:30,488 root.LicenseEngine started without redundancy.
2014-03-14 14:15:06,530 root.LicenseEngine stopped.
2014-03-14 14:15:07,659 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-14 14:15:07,789 root.LicenseEngine started without redundancy.
2014-03-14 14:15:08,005 root.Vendor (tidspssw) started.
2014-03-14 15:54:56,350 root.LicenseEngine stopped.
2014-03-14 15:54:56,940 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-14 15:54:56,974 root.LicenseEngine started without redundancy.
2014-03-14 15:54:57,083 root.Vendor (tidspssw) started.
2014-03-14 16:07:08,186 root.LicenseEngine stopped.
2014-03-14 16:07:09,182 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-14 16:07:09,225 root.LicenseEngine started without redundancy.
2014-03-14 16:07:09,350 root.Vendor (tidspssw) started.
2014-03-14 16:07:55,959 root.LicenseEngine stopped.
2014-03-14 16:07:56,543 root Version: 11.12.0.0 build 136897 (2013.08.27-08.45.28)
2014-03-14 16:07:56,586 root.LicenseEngine started without redundancy.
2014-03-14 16:07:56,717 root.Vendor (tidspssw) started.

15:23:11 (tidspssw) Server started on ctsgepc7 for:	CCS_CONNECTION_ALL 
15:23:11 (tidspssw) CCS_DEBUGGER	CCS_LINKER_FULL CCS_ISA_ALL	
15:23:11 (tidspssw) EXTERNAL FILTERS are OFF
15:29:46 (tidspssw) TCP_NODELAY NOT enabled
 0:00:53 (tidspssw) ERROR: Non-activation-capable daemon activation invoked with non-client-request event type
 3:04:41 (tidspssw) Lost communications with lmgrd. 
Socket disconnected by remote.
Exiting.
 3:04:41 (tidspssw) EXITING DUE TO SIGNAL 28 Exit reason 5
 3:09:15 (tidspssw) Server started on ctsgepc7 for:	CCS_CONNECTION_ALL 
 3:09:15 (tidspssw) CCS_DEBUGGER	CCS_LINKER_FULL CCS_ISA_ALL	
 3:09:15 (tidspssw) EXTERNAL FILTERS are OFF
 3:19:16 (tidspssw) TCP_NODELAY NOT enabled
10:56:11 (tidspssw) cannot create semaphore lock (Global\LM_tidspssw_SEMAPHORE): 5
10:56:11 (tidspssw) EXITING DUE TO SIGNAL 32 Exit reason 9
12:53:19 (tidspssw) cannot create semaphore lock (Global\LM_tidspssw_SEMAPHORE): 5
12:53:19 (tidspssw) EXITING DUE TO SIGNAL 32 Exit reason 9
12:53:21 (tidspssw) cannot create semaphore lock (Global\LM_tidspssw_SEMAPHORE): 5
12:53:21 (tidspssw) EXITING DUE TO SIGNAL 32 Exit reason 9
12:53:22 (tidspssw) cannot create semaphore lock (Global\LM_tidspssw_SEMAPHORE): 5
12:53:22 (tidspssw) EXITING DUE TO SIGNAL 32 Exit reason 9
12:54:13 (tidspssw) cannot create semaphore lock (Global\LM_tidspssw_SEMAPHORE): 5
12:54:13 (tidspssw) EXITING DUE TO SIGNAL 32 Exit reason 9
13:04:30 (tidspssw) cannot create semaphore lock (Global\LM_tidspssw_SEMAPHORE): 5
13:04:30 (tidspssw) EXITING DUE TO SIGNAL 32 Exit reason 9
 0:00:33 (tidspssw) ERROR: Non-activation-capable daemon activation invoked with non-client-request event type
 0:00:22 (tidspssw) ERROR: Non-activation-capable daemon activation invoked with non-client-request event type
14:15:07 (tidspssw) Lost communications with lmgrd. 
Socket disconnected by remote.
Exiting.
14:15:07 (tidspssw) EXITING DUE TO SIGNAL 28 Exit reason 5
14:15:07 (tidspssw) Server started on ctsgepc7 for:	CCS_CONNECTION_ALL 
14:15:07 (tidspssw) CCS_DEBUGGER	CCS_LINKER_FULL CCS_ISA_ALL	
14:15:07 (tidspssw) EXTERNAL FILTERS are OFF
14:25:09 (tidspssw) TCP_NODELAY NOT enabled
15:30:43 (tidspssw) Rereading license file...
15:30:43 (tidspssw) Server started on ctsgepc7 for:	CCS_CONNECTION_ALL 
15:30:43 (tidspssw) CCS_DEBUGGER	CCS_LINKER_FULL CCS_ISA_ALL	
15:30:43 (tidspssw) Updating feature CCS_CONNECTION_ALL
15:30:43 (tidspssw) Updating feature CCS_DEBUGGER
15:30:43 (tidspssw) Updating feature CCS_LINKER_FULL
15:30:43 (tidspssw) Updating feature CCS_ISA_ALL
15:30:43 (tidspssw) Rereading options file...
15:30:43 (tidspssw) ...Finished rereading
15:54:56 (tidspssw) Lost communications with lmgrd. 
Socket disconnected by remote.
Exiting.
15:54:56 (tidspssw) EXITING DUE TO SIGNAL 28 Exit reason 5
15:54:57 (tidspssw) Server started on ctsgepc7 for:	CCS_CONNECTION_ALL 
15:54:57 (tidspssw) CCS_DEBUGGER	CCS_LINKER_FULL CCS_ISA_ALL	
15:54:57 (tidspssw) EXTERNAL FILTERS are OFF
16:04:58 (tidspssw) TCP_NODELAY NOT enabled
16:07:08 (tidspssw) Lost communications with lmgrd. 
Socket disconnected by remote.
Exiting.
16:07:08 (tidspssw) EXITING DUE TO SIGNAL 28 Exit reason 5
16:07:09 (tidspssw) Server started on ctsgepc7 for:	CCS_CONNECTION_ALL 
16:07:09 (tidspssw) CCS_DEBUGGER	CCS_LINKER_FULL CCS_ISA_ALL	
16:07:09 (tidspssw) EXTERNAL FILTERS are OFF
16:07:56 (tidspssw) Lost communications with lmgrd. 
Socket disconnected by remote.
Exiting.
16:07:56 (tidspssw) EXITING DUE TO SIGNAL 28 Exit reason 5
16:07:56 (tidspssw) Server started on ctsgepc7 for:	CCS_CONNECTION_ALL 
16:07:56 (tidspssw) CCS_DEBUGGER	CCS_LINKER_FULL CCS_ISA_ALL	
16:07:56 (tidspssw) EXTERNAL FILTERS are OFF
16:17:58 (tidspssw) TCP_NODELAY NOT enabled
 0:00:32 (tidspssw) ERROR: Non-activation-capable daemon activation invoked with non-client-request event type
 0:00:18 (tidspssw) ERROR: Non-activation-capable daemon activation invoked with non-client-request event type
 0:00:47 (tidspssw) ERROR: Non-activation-capable daemon activation invoked with non-client-request event type
 0:00:34 (tidspssw) ERROR: Non-activation-capable daemon activation invoked with non-client-request event type

[Tue Mar 11 15:19:45 2014] [notice] ModSecurity for Apache/2.6.6 (http://www.modsecurity.org/) configured.
[Tue Mar 11 15:19:45 2014] [notice] ModSecurity: APR compiled version="1.4.5"; loaded version="1.4.5"
[Tue Mar 11 15:19:45 2014] [notice] ModSecurity: PCRE compiled version="8.12"; loaded version="5.0 13-Sep-2004"
[Tue Mar 11 15:19:45 2014] [warn] ModSecurity: Loaded PCRE do not match with compiled!
[Tue Mar 11 15:19:45 2014] [notice] ModSecurity: LIBXML compiled version="2.7.7"
[Tue Mar 11 15:19:45 2014] [notice] Child 21116: Child process is running
[Tue Mar 11 15:19:45 2014] [notice] Child 21116: Acquired the start mutex.
[Tue Mar 11 15:19:45 2014] [notice] Child 21116: Starting 10 worker threads.
[Tue Mar 11 15:19:46 2014] [notice] Child 21116: Starting thread to listen on port 8090.
[Tue Mar 11 15:22:22 2014] [error] [client ::1] File does not exist: C:/Program Files (x86)/FlexNet Publisher License Server Manager/web/images/popup/blank.html, referer: http://localhost:8090/systeminfo?vendor=&licenseTab=&selected=&expiredPassword=true
[Tue Mar 11 15:22:22 2014] [error] [client ::1] File does not exist: C:/Program Files (x86)/FlexNet Publisher License Server Manager/web/images/popup/resources, referer: http://localhost:8090/images/popup/blank.html
[Tue Mar 11 15:22:22 2014] [error] [client ::1] File does not exist: C:/Program Files (x86)/FlexNet Publisher License Server Manager/web/images/popup/resources, referer: http://localhost:8090/images/popup/blank.html
[Wed Mar 12 03:04:34 2014] [notice] Child 21116: Exit event signaled. Child process is ending.
[Wed Mar 12 03:04:34 2014] [warn] (OS 995)The I/O operation has been aborted because of either a thread exit or an application request.  : winnt_accept: Asynchronous AcceptEx failed.
[Wed Mar 12 03:04:35 2014] [notice] Child 21116: Released the start mutex
[Wed Mar 12 03:04:36 2014] [notice] Child 21116: All worker threads have exited.
[Wed Mar 12 03:04:36 2014] [notice] Child 21116: Child process is exiting
[Wed Mar 12 03:09:16 2014] [notice] ModSecurity for Apache/2.6.6 (http://www.modsecurity.org/) configured.
[Wed Mar 12 03:09:16 2014] [notice] ModSecurity: APR compiled version="1.4.5"; loaded version="1.4.5"
[Wed Mar 12 03:09:16 2014] [notice] ModSecurity: PCRE compiled version="8.12"; loaded version="5.0 13-Sep-2004"
[Wed Mar 12 03:09:16 2014] [warn] ModSecurity: Loaded PCRE do not match with compiled!
[Wed Mar 12 03:09:16 2014] [notice] ModSecurity: LIBXML compiled version="2.7.7"
[Wed Mar 12 03:09:17 2014] [notice] Child 1724: Child process is running
[Wed Mar 12 03:09:17 2014] [notice] Child 1724: Acquired the start mutex.
[Wed Mar 12 03:09:17 2014] [notice] Child 1724: Starting 10 worker threads.
[Wed Mar 12 03:09:17 2014] [notice] Child 1724: Starting thread to listen on port 8090.
[Fri Mar 14 14:15:04 2014] [notice] Child 1724: Exit event signaled. Child process is ending.
[Fri Mar 14 14:15:04 2014] [warn] (OS 995)The I/O operation has been aborted because of either a thread exit or an application request.  : winnt_accept: Asynchronous AcceptEx failed.
[Fri Mar 14 14:15:05 2014] [notice] Child 1724: Released the start mutex
[Fri Mar 14 14:15:06 2014] [notice] Child 1724: All worker threads have exited.
[Fri Mar 14 14:15:06 2014] [notice] Child 1724: Child process is exiting
[Fri Mar 14 14:15:09 2014] [notice] ModSecurity for Apache/2.6.6 (http://www.modsecurity.org/) configured.
[Fri Mar 14 14:15:09 2014] [notice] ModSecurity: APR compiled version="1.4.5"; loaded version="1.4.5"
[Fri Mar 14 14:15:09 2014] [notice] ModSecurity: PCRE compiled version="8.12"; loaded version="5.0 13-Sep-2004"
[Fri Mar 14 14:15:09 2014] [warn] ModSecurity: Loaded PCRE do not match with compiled!
[Fri Mar 14 14:15:09 2014] [notice] ModSecurity: LIBXML compiled version="2.7.7"
[Fri Mar 14 14:15:10 2014] [notice] Child 8284: Child process is running
[Fri Mar 14 14:15:10 2014] [notice] Child 8284: Acquired the start mutex.
[Fri Mar 14 14:15:10 2014] [notice] Child 8284: Starting 10 worker threads.
[Fri Mar 14 14:15:10 2014] [notice] Child 8284: Starting thread to listen on port 8090.
[Fri Mar 14 15:54:54 2014] [notice] Child 8284: Exit event signaled. Child process is ending.
[Fri Mar 14 15:54:54 2014] [warn] (OS 995)The I/O operation has been aborted because of either a thread exit or an application request.  : winnt_accept: Asynchronous AcceptEx failed.
[Fri Mar 14 15:54:55 2014] [notice] Child 8284: Released the start mutex
[Fri Mar 14 15:54:56 2014] [notice] Child 8284: All worker threads have exited.
[Fri Mar 14 15:54:56 2014] [notice] Child 8284: Child process is exiting
[Fri Mar 14 15:54:58 2014] [notice] ModSecurity for Apache/2.6.6 (http://www.modsecurity.org/) configured.
[Fri Mar 14 15:54:58 2014] [notice] ModSecurity: APR compiled version="1.4.5"; loaded version="1.4.5"
[Fri Mar 14 15:54:58 2014] [notice] ModSecurity: PCRE compiled version="8.12"; loaded version="5.0 13-Sep-2004"
[Fri Mar 14 15:54:58 2014] [warn] ModSecurity: Loaded PCRE do not match with compiled!
[Fri Mar 14 15:54:58 2014] [notice] ModSecurity: LIBXML compiled version="2.7.7"
[Fri Mar 14 15:54:59 2014] [notice] Child 5456: Child process is running
[Fri Mar 14 15:54:59 2014] [notice] Child 5456: Acquired the start mutex.
[Fri Mar 14 15:54:59 2014] [notice] Child 5456: Starting 10 worker threads.
[Fri Mar 14 15:54:59 2014] [notice] Child 5456: Starting thread to listen on port 8090.
[Fri Mar 14 16:07:06 2014] [notice] Child 5456: Exit event signaled. Child process is ending.
[Fri Mar 14 16:07:06 2014] [warn] (OS 995)The I/O operation has been aborted because of either a thread exit or an application request.  : winnt_accept: Asynchronous AcceptEx failed.
[Fri Mar 14 16:07:07 2014] [notice] Child 5456: Released the start mutex
[Fri Mar 14 16:07:08 2014] [notice] Child 5456: All worker threads have exited.
[Fri Mar 14 16:07:08 2014] [notice] Child 5456: Child process is exiting
[Fri Mar 14 16:07:10 2014] [notice] ModSecurity for Apache/2.6.6 (http://www.modsecurity.org/) configured.
[Fri Mar 14 16:07:10 2014] [notice] ModSecurity: APR compiled version="1.4.5"; loaded version="1.4.5"
[Fri Mar 14 16:07:10 2014] [notice] ModSecurity: PCRE compiled version="8.12"; loaded version="5.0 13-Sep-2004"
[Fri Mar 14 16:07:10 2014] [warn] ModSecurity: Loaded PCRE do not match with compiled!
[Fri Mar 14 16:07:10 2014] [notice] ModSecurity: LIBXML compiled version="2.7.7"
[Fri Mar 14 16:07:11 2014] [notice] Child 5148: Child process is running
[Fri Mar 14 16:07:11 2014] [notice] Child 5148: Acquired the start mutex.
[Fri Mar 14 16:07:11 2014] [notice] Child 5148: Starting 10 worker threads.
[Fri Mar 14 16:07:11 2014] [notice] Child 5148: Starting thread to listen on port 8090.
[Fri Mar 14 16:07:53 2014] [notice] Child 5148: Exit event signaled. Child process is ending.
[Fri Mar 14 16:07:53 2014] [warn] (OS 995)The I/O operation has been aborted because of either a thread exit or an application request.  : winnt_accept: Asynchronous AcceptEx failed.
[Fri Mar 14 16:07:54 2014] [notice] Child 5148: Released the start mutex
[Fri Mar 14 16:07:55 2014] [notice] Child 5148: All worker threads have exited.
[Fri Mar 14 16:07:55 2014] [notice] Child 5148: Child process is exiting
[Fri Mar 14 16:07:58 2014] [notice] ModSecurity for Apache/2.6.6 (http://www.modsecurity.org/) configured.
[Fri Mar 14 16:07:58 2014] [notice] ModSecurity: APR compiled version="1.4.5"; loaded version="1.4.5"
[Fri Mar 14 16:07:58 2014] [notice] ModSecurity: PCRE compiled version="8.12"; loaded version="5.0 13-Sep-2004"
[Fri Mar 14 16:07:58 2014] [warn] ModSecurity: Loaded PCRE do not match with compiled!
[Fri Mar 14 16:07:58 2014] [notice] ModSecurity: LIBXML compiled version="2.7.7"
[Fri Mar 14 16:07:59 2014] [notice] Child 4588: Child process is running
[Fri Mar 14 16:07:59 2014] [notice] Child 4588: Acquired the start mutex.
[Fri Mar 14 16:07:59 2014] [notice] Child 4588: Starting 10 worker threads.
[Fri Mar 14 16:07:59 2014] [notice] Child 4588: Starting thread to listen on port 8090.
[Sat Mar 15 07:44:52 2014] [error] [client 183.221.12.212] File does not exist: C:/Program Files (x86)/FlexNet Publisher License Server Manager/web/science
[Sun Mar 16 03:15:15 2014] [error] [client 183.221.13.196] File does not exist: C:/Program Files (x86)/FlexNet Publisher License Server Manager/web/science

  • Hi Louis,

    a few questions.  What exact version of ccs are you using.  Also, is my understanding correct on the server machine you can access a license?  Is this issue only on the remote machines?

    Any details would help.  Also, if so, is on the remote machines, how are you pointing ccs to the license?  Have you double checked the firewalls/proxys/permissions?  Also that you are using 8080?

    Have you tried restarting the service?

    Best Regards,
    Lisa

  • Hello Lisa, 

    Thank you for the swift reply !

    I have used the version that was shipped to me in a DVD, which is CCSv5.3. I've also tried downloading CCSv5.4, however the result is exactly the same. 

    This issue occurs on more than on remote machine. In fact, it occurs with all of the remote machines, and I haven't been able to run the software successfully on any of our computers.

    As for the remote machines, once in CCSv5, I went into the License management menu found under the Help menu, and added the license server's domain name (which is hosted on the EPFL's network). The port that is in use is 27000 as outlined in the FlexNet license administration web interface. The result is 27000@domainname.epfl.ch. I've also tried using the IPv4 address of the server directly instead of its domain name, but this doesn't seem to change much.

    As for the firewalls, I've double checked them both client side and server side. I've even tried to see if turning the firewalls off on both computers changed anything, but it hasn't changed anything either. What do you mean by proxies ? Permissions seemed fine as well.

    For some reason, the Flexnet license administration interface is not accessed through 8080, but through 8090 instead (I can only access the interface through domainname.epfl.ch:8090). Is this normal ? On the wiki it is stated that port 8080 should be the one used to access the interface.

    I have restarted the service several times already.

    Hope this helps. Thanks for the continued support ! Cheers,

    Louis

  • Hi Louis,

    no problem, although non of us are flexnet experts and in fact we have an internal license system we use which makes it even harder.

    I would try using 8080.  I would also double check the 27000 .. use 8080 there instead or make sure it is not something other than 27000.

    Do you use the GUI to setup the server? Could you send screen captures?

    Best regards,

    Lisa

  • Hi Lisa,

    I can't even begin to imagine how complicated it must be. I understand if FlexNet isn't your expertise either, but I hope we'll be able to figure it out somehow.

    Alright, how do I configure the service to go through port 8080 and not 8090 ? Is this done in the license manager's GUI ? I'll take a look at the 27000 port and also try the 8080 port to see if it takes us anywhere, then I will come back to you with the results (tomorrow I'm afraid, I'm going to have to leave the lab soon).

    What I use to setup the server is the online GUI that can be accessed through the 8090 port of our server's address. You will find attached a screenshot of said interface. When I try to launch lmgrd.exe or lmadmin.exe from the server, nothing happens.

    Best regards,
    Louis

  • Hi Louis,

    try in the vedon daemon configuration ...

    Best Regards,

    Lisa

  • Hi Lisa, I've managed to get out system working somehow ! Here's what I did :

    1. I re installed the license manager to see if it could change anything (and I configured it this time to the 8080 port for accessing the GUI).

    2. I realized that we needed to open the appropriate ports (8080, the license manager port, as well as the vendor daemon's port which can be found in the vendor daemon configurations) for several of the programs contained within the FLEXnet installation. Thus the three aforementioned ports were open for the lmadmin service, as well as these programs : lmadmin.exe, lmgrd.exe, lmutil.exe, tidspssw.exe

    For some reason it works like a charm now. Thanks a lot for your input !

    Best regards,
    Louis

  • Hi Louis,

    Great, glad to hear things are up and running.

    Thanks for the update and all the best with development.

    Best Regards,

    Lisa