This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I was using CCS5.3, cgtool 6.4.2, C64x+ Megamodule Cycle Accurate Simulator, to do cache analysis. I followed the instructions in CCS help 3.9.5.1 to get profile data. I selected "--gen_profile_info" compiler option.
When I ran my application, it didn't generate the .pdat file and the program never stopped. Did I miss anything?
Thanks and regards,
Jianzhong
Please see my code below. The second last line of code in main() was executed.
int main(int argc, char *pp_argv[])
{
...
...
/* print the last error message received by the error handler */
print_last_message(&g_exec.errcb_data);
/* close the executive layer */
exec_close(&g_exec);
print_exit_status_to_file(err); -> This line is executed.
return (err);
}
Thanks,
Jianzhong
To confirm:
jianzhongxu said:print_exit_status_to_file(err); -> This line is executed.
It returns from this function call but gets stuck on 'return (err);' ?
In fact, when stepped through the code, it passed the last line and then I got the following error message:
Can't find a source file at "/tmp/TI_MKLIBHEeM99/SRC/boot.c"
That's not really an error. Basically you are halted inside the boot routine from the run-time library. Aarti explains it in detail in this post:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/230662/811582.aspx#811582
What is curious is why you end up there if you are not doing a reset of some sort. Most likely there is some kind of bug in the application. If you only see this when enabling --gen_profile_info, it could be some memory allocation issue. Please provide a reproducible test case and I can investigate further.
Thanks
ki