This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIVAWARE How to build Guideline.



 After unsuccesful DM-TM4C129 application I try if someone can share tip and tricks to have an example from TIVAWare imported and build without pain.

 How to interpret linker errors and why symbol of a prepackaged project remain undefined.
 Why a project don't build.

 How to set property of project.

 How and where to include library like LWIP and FS

  • The examples for DK-TM4C129x that come with Tivaware should build out of the box without errors. You should be able to simply import the project into CCS (Project->Import CCS Projects) and build it.

    Typically "unresolved symbol" errors coming from the linker means that you may not be linking in a desired library. Libraries are sepcified under Project Properties->Build->Linker->File Search Path. You can take a look at any of the examples in Tivaware to see how these are specified.

    If you are getting errors with any of the examples, please let us know specifically which example. A screenshot of the error or a text file with the full build output in CCS console will also be helpful in understanding the error.

  • AartiG said:
    Typically "unresolved symbol" errors coming from the linker means that you may not be linking in a desired library. Libraries are sepcified under Project Properties->Build->Linker->File Search Path. You can take a look at any of the examples in Tivaware to see how these are specified.

     Hi Aartig, I appreciate your explain of linker error but after approaching 40 year of computer experience when compiler don't produce obj nothing link ;)

     On CCS beta there was a widget to guide project setting, the goal of this thread was to build a guide of how to set various parameter and libraries and prepare a project from scratch.

     About import, I am sorry it doesn't work on Linux version!