This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
I am trying to open an existing CCS3.3 project in CCS5.1.
I have imported the project successfully, but upon building it, I get the following errors:
C:\ti\ccsv5\utils\bin\gmake -k all
'Building file: Z:/Projects/DSP
'NHST' is not recognized as an internal or external command,
operable program or batch file.
gmake: *** [V2AcqSyscfg.cmd] Error 1
gmake: Target `all' not remade because of errors.
Now I've done some research here and found the following threads, which are close, but don't solve my issue:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/168935.aspx
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/215561.aspx
I'm mostly concerned with the line that NHST is not recognized as a command.
Please let me know if you can assist, and if you require any additional info.
Thanks.
Cam Buskell said:C:\ti\ccsv5\utils\bin\gmake -k all
'Building file: Z:/Projects/DSP
'NHST' is not recognized as an internal or external command,
It looks like some path issue. 'Z:/Projects/DSP' looks like some truncated path to a source file. Where are the source files located?
Ah, no that's not the correct directory.
There's a few more sub folder levels:
Z:\Projects\DSP&NewHighSpeedTelemetry\ . . . \TWRec0.3 - CCS5
Does the ampersand affect the file path?
How do I change the build path to the correct one?
Cam Buskell said:Does the ampersand affect the file path?
Yes. Ampersands and other "special" characters can cause issues.
Similar issue found here:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/260781.aspx
Cam Buskell said:How do I change the build path to the correct one?
The build tools does not seem to handle such special characters. I would recommend changing the name of that folder if possible.
ki
Copying the directory to hard drive and renaming solves this issue.
I now have a related issue:
In building the project, I get an access is denied failure
>> Compilation failure
gmake: *** [C:/ . . . /AcqSysHighLeeSpecEn.obj] Error 1
'Building file: C:/ . .. /TWRec0.3/AcqSysProcessing.c'
gmake: *** Access is denied.
What does this mean? there are no permission issues on my local drive.
Furthermore, whenever I build the project, it times out at this error.
Cam Buskell said:gmake: *** Access is denied.
Two common causes of this error:
-Some antivirus software is overly aggressive. Kaspersky is one that has caused problems in the past. Try disabling it as a test.
-junctions (soft-links)
Thanks for the help. I ended up cleaning the project and then building from there.
I had to do it file by file however, but once it worked, it was fine going forward.
Thanks.