Hi,
I recently started working with the OMAP L137 EVM and code composer studio. In an effort to learn how to use the DSP/BIOS (5.33) I started going through the tutorial in the DSP/BIOS configuration tool. Unfortunately CCS is giving me some problems:
First off, when I go to create a configuration file for the DSP/BIOS, I go to File->New->DSP/BIOS Configuration, however when I click it nothing happens! This doesn't seem to be a huge deal since I can just open up the DSP/BIOS graphical configuration tool by itself, however maybe it suggests some larger problem.
Second, after creating a project (I'm following along with the tutorial doing the clk project) and adding a few files, I then need to add the DSP/BIOS configuration file (.tcf) to the project. When I go to Project->Add files to project and I get the explorer window to browse to the file to add, there is no option to add the .tcf file type, and for that matter .h files either! When I have the browser window display all of the file types, and select the .tcf file, CCS just adds it to the documents folder in the project and not the DSP/BIOS configuration folder. (It also does this for the header (.h) files).
What do y'all think could be the issue? Thanks for your help.
Chris