This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everyone,
i'm using code composer studio v6.1 with an EVM AM437x and i get next error try to debug a program in ARM Cortex A9:
"Cannot read System Setup data from XML file D:\hell_oword_new\hello_test\targetConfigs\AM3359.ccxml
Could not compile SQL statement (unable to open database file)
If this continues, please run fsclean located at E:\ccs\ccsv6\ccs_base\common\bin\"
After choose simulators xds100v2 ,click verify,you can see
"Could not compile SQL statement (unable to open database file)
If this continues, please run fsclean located at E:\ccs\ccsv6\ccs_base\common\bin\"
Please advise what to do
Thank you
Billy
same problem,tried on my two computer with Win8.1 64 bit
my ccxml file code:
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="configuration_0">
<instance XML_version="1.2" desc="TI MSP430 USB1" href="connections/TIMSP430-USB.xml" id="TI MSP430 USB1" xml="TIMSP430-USB.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="TI MSP430 USB1">
<instance XML_version="1.2" href="drivers/msp430_emu.xml" id="drivers" xml="msp430_emu.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="MSP430FR5969" href="devices/MSP430FR5969.xml" id="MSP430FR5969" xml="MSP430FR5969.xml" xmlpath="devices"/>
</platform>
</connection>
</configuration>
</configurations>