This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I was wondering if it were possible to do an unattended install of CCS for msp430 based setups in linux. If it is possible would I also be able to skip the error message about libudev.so.0 because I don't want to implement the fix since I don't use GUI composer.
Kevin
Hi Kevin,
Kevin Freeman said:I was wondering if it were possible to do an unattended install of CCS for msp430 based setups in linux. If it is possible would I also be able to skip the error message about libudev.so.0 because I don't want to implement the fix since I don't use GUI composer.
Nope, I really don't think you would be able to skip the error messages.
Regards,
Gautam
AndyW said:You should be able to use the --mode unattended and --prefix <installdir> command line flags to do an unattended install. I think it skips the dependency check.
Nice and what about the errors and warnings (turn-off antivirus & firewall) ?
Regards,
Gautam
The unattended mode will run without any popups. If there are errors, you need to check the log files.