This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I have some difficulties connecting to my F28121 eZdsp board. I tried connecting using the on-board JTAG emulator and external XDS510 USB emulators, and faced error messages in SDconfig3.1 (I use ccsv3.1 and xds510 usb emulator rev A serial #2004/01-013)
for XDS510USB:
** Emulator Test **
$$ EmuProductName=XDS510USB
$$ EmuPortAddr=0x510
$$ EmuPortMode=USB
$$ ProductId=510
$$ ProductVersion=84
** Emulator Scan Test
ERROR >> JTAG IR scan test failed
>> Check power to your emulator/eZdsp
>> Then check your port mode/address
phuong vu
Hi all, (posted question)
+ I have some difficulties connecting to my F28121 eZdsp board. I tried connecting using the on-board JTAG emulator and external XDS510 USB emulators, and faced error messages in SDconfig3.1 (I use ccsv3.1 and xds510 usb emulator rev A serial #2004/01-013)
for XDS510USB:
** Emulator Test **
$$ EmuProductName=XDS510USB
$$ EmuPortAddr=0x510
$$ EmuPortMode=USB
$$ ProductId=510
$$ ProductVersion=84
** Emulator Scan Test
ERROR >> JTAG IR scan test failed
>> Check power to your emulator/eZdsp
>> Then check your port mode/address
+In setup ccs: F2812 XDS510USB Emulator
+ error notice in ccs when connect betwen F2812 and XDS510USB Emulator
Error connecting to the target:
Error 0x80000200/-1135
Fatal Error during: OCS,
Unrecoverable emulation error
Sequence ID: 0
Error Code: -1135
Error Class: 0x80000200
I/O Port = 510
Board Name: F2812 XDS510USB Emulator
Cpu Name: cpu_0
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
phuong vu
Phong,
Have you been able to connect previously?
Could you check the XCLKOUT pin to see if it toggles at the correct frequency?
Also check power and ground.
If the device is in a socket, check that it is seated properly and some pins didn't become disconnected.
Regards,
-Lori
Lori,
Could you tell me how to check the the XCLKOUT pin and check power and ground.
my card ezdsp is not in a socket. it fixed in card.
Regards,
phuong
Dear,
I connected 2 times and loaded program to target, but the last time when i`m using, i touch the USB cable and my PC show the report that not connecting to target anymore.
I do it again but the error appears all the times.
I live in Viet Nam, can I send my emulator to your support customer center to fix? If yes, how can i do it?
It`s great if you can give me some solutions.
Thank a lot!
Best regards,