Other Parts Discussed in Thread: CC3200
Device 'Cortex M.CC3200' is not recognized. Please install the device descriptor, or select the closest match from the supported devices.
"Description Resource Path Location Type
This project was created for a device that is not currently recognized: Cortex M.CC3200. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the device descriptor, or migrate the project to the closest match from the supported devices by adjusting project properties. saferagingtest project Problems"
Host: Linux Mint 16 x64 Kernel 3.11.0-12
CCS Version: 6.0.1.00040
Device: CC3200
When installing CCS the option for "CC32xx Device support" was not among the checkboxes of things I could install. I did install TI-RTOS for SimpleLink and the TI ARM Compiler in the CCS App Center to no avail. Any solution for this? I can't even build a project.