Other Parts Discussed in Thread: MSP430F1611, MSP430F5418A
Hi, I have a problem running the firmware on msp430f1611 under CCS version 5.5.0.00077
compiler version: TI v4.2.1.
When I load the firmware always pops up the message MSP430: Error connecting to the target: Unknown device). But after pushing the button "retry" loading works .
When I am trying to stop (suspend) the running firmware my debugger stops,
but the micro still running and all data in the debugger is wrong (message is: MSP430: Trouble Halting Target CPU: Internal error). Sometimes this command works, but most of the times - no. Else I can't reset the firmware (message: MSP430: Failed Soft reset: Could not reset device).
Note:
I use the same version of CCS with msp430f5418a without any problem.
I will appreciate for any help.
Thanks,
Michael Golod