Hi,
I've copied a motorware project that I've been working on for a long time from one pc to another, but when I try to build I get the error message fatal error #1965: cannot open source file "user.h"
I'm guessing the problem is related to file paths or workspace location but I'd like some guidance on the correct steps to correct the problem.
On the original pc the Linked Resources show PARENT_LOC at C:\Users\Geoff\workspace_v6.0, PROJECT_LOC at c:\ti\motorware\motorware_1_01_00_12_jwcamera\solutions\........., and WORKSPACE_LOC at C:\Users\Geoff\workspace_v6.0
On the new pc the Linked Resources show PARENT_LOC at C:\Users\Geoff\workspace_v5.3, PROJECT_LOC at C:\Users\Geoff\workspace_v5.3\proj_lab13b_test, and WORKSPACE_LOC at C:\Users\Geoff\workspace_v5.3
it also has another entry ORIGINAL_PROJECT_ROOT at c:\ti\motorware\motorware_1_01_00_12_jwcamera\solutions\.........
Clearly these are different, so is this the problem and what do I need to change ? Is there any problem using a 6.0 project in 5.3 ?
Thanks,
Geoff