This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
TI has provided the CCS interface function for us, such as connect,load,run,step,set breakpoints,clear breakpoints and so on. And we developed debugging software in the CCS based on a PCIE bus or internet, which can connect with c6678 board,can download program to the board, and debug program on the board. Now the software has been delivered to users. After they used our K1 debugging software,there are some feedback problems.
Run to line, step over, and assembly step over are not good or not supported. Users want to be able to use these features, but because TI only opens to us step, so our software can't modify "run to line, step over, assembly step over", they are background operation of CCS. We have no way to use our own code to implement these functions, could TI open these interface functions to us?
Thanks,
Regards
Ah I get it now. Sorry for not understanding.
You earlier said "TI has provided the CCS interface function for us". Which interface functions are you using? DSS?
Thanks
ki
Na Li1 said:We have CCS interface function project , a VS2010 project, and *.dvr is its result of compiling the project. *.dvr is like ti\ccsv6\ccs_base\emulation\drivers\*.dvr. The VS2010 project only has connect,disconnect,load,run,step,set breakpoint,clear breakpoint, but don't have run to line,step over assembly step over. We hope these function,run to line,step over assembly step over, we can program to realize these function.
I see that you started a new thread with this question. I moved that to the C6000 Multi-core forum as I think it might be more appropriate there.
http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/405807
Hi,
It is not DSS. It's TI only make for our company. We use software to realize the middleware between CCS and board. The interface function is some source file, gti file and CMakeList.txt files, According to this files, I new a VS2010 project, It compile these files to a *.dvr file. The source file include some .c, such as GTISkeleton.c. The gti file include some .h, such as gti.h. And the CMakeList is the build rule.
Thanks,
Regards