Hi!
I initially installed CCS v4 on Windows 7 64bit machine, however, the CCS v4 had multiple issues with displaying its UI and it was not possible to access configuration settings for the compiler. Then I tried to install the CCS in the VM on the same machine which was 32bit Vista. This worked, but the emulator (XDS510) worked really slow, possibly due to USB mapping to the VM. Finally I tried to install the CCS v4 on to 32bit Windows 7 machine and the UI seems to be working fine. However, when I tried to connect to the board, the DebugServer reports, that I dont have a license to run the CCS. After finally finding an OS, where CCS seems to work, how can I now use the EVM?
Does the CCS v4 trial also time out for XDS100 emulators and EVM boards?
Thanks!
Atmapuri