This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Helllo everyone,
Environment Info:
OS : Windows 7
LP : CC3200
Software : CCS v6.0.0
When I plugged in my CC3200 LP into my system, system got hardware exception and restarted after completing scan for memory dump. After this I have opened my project in CCS but unfortunately one of my C file is showing no content, however file size is exactly same as before. Notepad++ is showing many "NULL" on screen. Does the file get corrupted? Is there any way I can get it back? Code inside file is very important for me.
Thanks,
Niral
Try to open it with notepad (not notepad ++)? Did you set the compiler to generate assembly interleaved with source code (check the release/debug directory). If so, you could retrieve your source from those files.
Did you have your files on a network drive? Usually, the IT makes backups of network drives. If so, you could ask them to restore the files.
Hi stevenh,
I have only corrupted source file (.c). I have tried opening file with notepad as well but couldn't get anything.
Niral
Hi Gautam,
We are working with various lauchpad of TI since last 1.5 years. Such an incident never happened with us that is why we don't keep back up of files. However we'll start backing up our files from now on.
Niral