This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a custom board with C6678 and CCS v6.1 I have set up the memory map correctly. I can Load Memory with a file, but I can't get the Fill Memory function to work. I'm trying to fill DDR3 with 0's starting at 0x80000000. I have 1 GB of memory there, and I can write each individual word location to 0 manually by double clicking it and setting it to 0, so it physically can work. What am I doing wrong?
Mike
I tried L2 sram and it also didn't work,
But, I after playing around with it, I found out that the Length parameter is expected in hex. I was entering 0x100 in the box and it didn't work, simple did nothing, no error indication. If I enter 10, it does 16 values. So the box needs a hex value, without the 0x in front. Now it seems to work.
Thanks. Mike