I am using the RM48 USB Stick Development Kit which includes Cortex R4F and XDS100v2 USB Debug Probe.
I want to use the Trace Analyzer with CCS Version: 6.1.0.00104.
I began to create a RM48 Target Configuration file and the test of connection is OK.
Then I entered in the debug mode.
Then I set a Function Profiling Configuration but I got the following error message:
Could not run analyzer on Cortex R4. Cause:
Read device ID did not match the device descriptions available.
Possible reasons:
(1) Target is not connected
(2) Trace support for the device is not available in the version of the software.
Where is the mistake?
Thanks for your help
Jerome