This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How can we confirm that the project in CCS is using elf FastRTS library instead of default RTS library?

For TI C64x+ and the compiler is  ti-cgt-c6000_8.0.1, i want to know whether the compiler is using the already linked ELF FastRTS library or is it using the default ELF RTS library. Can you please provide me with some method by which i can verify the same?

In the .map file i can see both ELF RTS and ELF FastRTS .obj files, but I want to confirm that my FastRTS library is working fine and the compiler is prioritising it over the RTS library.