This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The compiler is generating the following warning:
warning #10210-D: creating ".sysmem" section with default size of 0x400; use the -heap option to change the default size
I thought .sysmem was replaced with .esysmem, so why is a .sysmem section being created?
Also, isn't .esysmem/sysmem only used for dynamic memory allocation? My program is not performing any dynamic memory allocation, so why is either of those two section being created?
Thanks,
Stephen,
The memory map refers to memory.obj for that section. The code shown below is the reason for the creation of the .sysmem section.
Why does the compiler allow an unsized array in the Run Time Library?
In memory.c (runtime system libary):
/*****************************************************************************/
/* Declare the memory pool as a .usect called .sysmem. The size of the */
/* section .sysmem is determined by the linker via the -heap option */
/*****************************************************************************/
#pragma DATA_SECTION(_sys_memory, ".sysmem")
int _sys_memory[];
stevenh said:I thought .sysmem was replaced with .esysmem
The section .sysmem is used for malloc and related functions. The section .esysmem is used for far_malloc and related functions.
stevenh said:My program is not performing any dynamic memory allocation, so why is either of those two section being created?
I don't know. Is malloc the only unusual thing that appears in the map file? Do you see unexpected printf calls, or anything else like that?
Thanks and regards,
-George
Hello George,
From my previous post I thought I understood why the sysmem section was showing up, i.e.
#pragma DATA_SECTION(_sys_memory, ".sysmem")
int _sys_memory[];
The original reason for my question was because of the "creating .sysmem section..." warning.
I never examined the memory map file that carefully; However, I am certain that my code doesn't contain malloc.
I wouldn't be able to tell if something strange was showing up because some functions use other function, however, I don't think any of the rts functions in my code are using malloc. The only rts functions I am using in my code (that I can remember) are memset, memcpy and sprintf.
Stephen
There is no method to automatically exclude malloc from the build.
Here is a technique which can show you where malloc is getting called. Here is the general idea:
All of the malloc functions are in the module memory.obj. These commands extract it from the library into its own file, then remove it from the library. Perform these commands from the command line in the \lib directory that contains the RTS libraries.
% ar2000 -x rts2800_ml.lib memory.obj % ar2000 -d rts2800_ml.lib memory.obj ==> building archive 'rts2800_ml.lib'
Now link as usual. You will see one or more error messages similar to ...
undefined first referenced symbol in file --------- ---------------- _malloc file.obj
That file contains a call to malloc. It is up to you to determine why that call is present and to remove it.
It is best to put the RTS library back the way it was. These commands do that ...
% ar2000 -r rts2800_ml.lib memory.obj ==> building archive 'rts2800_ml.lib' % del memory.obj
More information on the archiver ar2000 can be found in the C2000 assembly tools manual.
Thanks and regards,
-George
Hello George,
Thanks.
I did what you said (see below). I had to do it twice since the first time the linker output referred to the new_.obj file.
The final linked result from the sample project I previously at attached is as follows:
undefined first referenced symbol in file --------- ---------------- operator new(unsigned long) ./main.obj
I included both the c++ code and its associated disassembly (from the debugger) below. A pointer to __sti___6_main_c_d7ce1b44 (at the bottom of the disassembly) is located in the pinit table. __sti___6_main_c_d7ce1b44 calls the object's constructor.
I stepped through program and found out that "new" (i.e. LCR operator new) is never called (because XAR4 != 0) in the constructor (i.e. Test::Test():) , so what is the purpose of the call to "new"?
If I remove constructor from the program, the call to "new" goes away
C++ Code:
/* * main.c */ class Test { public: long int a; long int b; int x[10]; Test(void); void aTest(void); }; Test::Test(void) { int i; a=1000000000l; b=1000000000l; for(i=0;i<10;i++) { x[i] = i; } } void Test::aTest(void) { a = 2l; b = 3l; } Test TestIt; int main(void) { TestIt.aTest(); return 0; }
Assmebly Code (from debugger):
main(): 32021d: 8F008400 MOVL XAR4, #0x008400 32021f: 76720247 LCR aTest 44 return 0; 320221: 9A00 MOVB AL, #0x0 45 } 320222: 0006 LRETR 17 { Test::Test(): 320223: FE04 ADDB SP, #4 320224: A842 MOVL *-SP[2], XAR4 320225: 0642 MOVL ACC, *-SP[2] 320226: ED07 SBF C$L1, NEQ 320227: 020E MOVB ACC, #14 320228: 76720277 LCR operator new 32022a: A8A9 MOVL @ACC, XAR4 32022b: A842 MOVL *-SP[2], XAR4 32022c: EC18 SBF C$L3, EQ 20 a=1000000000l; C$L1: 32022d: 8A42 MOVL XAR4, *-SP[2] 32022e: 28A9CA00 MOV @AL, #0xca00 320230: 28A83B9A MOV @AH, #0x3b9a 320232: 1EC4 MOVL *+XAR4[0], ACC 21 b=1000000000l; 320233: 8A42 MOVL XAR4, *-SP[2] 320234: 1ED4 MOVL *+XAR4[2], ACC 23 for(i=0;i<10;i++) 320235: 2B43 MOV *-SP[3], #0 320236: 9243 MOV AL, *-SP[3] 320237: 520A CMPB AL, #0xa 320238: 630C SB C$L3, GEQ 25 x[i] = i; C$L2: 320239: 8A42 MOVL XAR4, *-SP[2] 32023a: 3B01 SETC SXM 32023b: 8543 MOV ACC, *-SP[3] 32023c: 8843 MOVZ AR6, *-SP[3] 32023d: 560100A4 ADDL @XAR4, ACC 32023f: 7EE4 MOV *+XAR4[4], AR6 23 for(i=0;i<10;i++) 320240: 0A43 INC *-SP[3] 320241: 9243 MOV AL, *-SP[3] 320242: 520A CMPB AL, #0xa 320243: 64F6 SB C$L2, LT 27 } C$L3: 320244: 8A42 MOVL XAR4, *-SP[2] 320245: FE84 SUBB SP, #4 320246: 0006 LRETR 30 { Test::aTest(): 320247: FE02 ADDB SP, #2 320248: A842 MOVL *-SP[2], XAR4 31 a = 2l; 320249: 8A42 MOVL XAR4, *-SP[2] 32024a: 0202 MOVB ACC, #2 32024b: 1EC4 MOVL *+XAR4[0], ACC 32 b = 3l; 32024c: 8A42 MOVL XAR4, *-SP[2] 32024d: 0203 MOVB ACC, #3 32024e: 1ED4 MOVL *+XAR4[2], ACC 33 } 32024f: FE82 SUBB SP, #2 320250: 0006 LRETR 35 Test TestIt; __sti___6_main_c_d7ce1b44(): 320251: 8F008400 MOVL XAR4, #0x008400 320253: 76720223 LCR Test 320255: 0006 LRETR
Your problem, and some suggested solutions, is discussed in this thread. Keep in mind that, at the present time, COFF ABI is the only ABI provided by the C2000 compiler. EABI, which is the best solution to this problem, will be available in a future release.
Thanks and regards,
-George
I would still like to know why the compiler allows an unsized array in the rts library? i.e.
In memory.c (runtime system libary):
/*****************************************************************************/
/* Declare the memory pool as a .usect called .sysmem. The size of the */
/* section .sysmem is determined by the linker via the -heap option */
/*****************************************************************************/
#pragma DATA_SECTION(_sys_memory, ".sysmem")
int _sys_memory[];
That code sets the global variable _sys_memory to the beginning of the section .sysmem. The section .sysmem is sized by the linker according to the value of the -heap option.
Thanks and regards,
-George
Yes, that fails in C++. But it works in C. And memory.c is C code.
Thanks and regards,
-George