Part Number: TMS320F28069
Tool/software: Code Composer Studio
It's my [F28069_CLA_C_lnk.cmd].
///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
_Cla1Prog_Start = _Cla1funcsRunStart;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */
RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
RAML6L8 : origin = 0x00E000, length = 0x001000 /* on-chip RAM block L3 */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */
FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */
IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000480, length = 0x000380 /* on-chip RAM block M1 */
CLARAM0 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
CLARAM1 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
RAML4 : origin = 0x00A000, length = 0x002000 /* on-chip RAM block L4 */
RAML5 : origin = 0x00C000, length = 0x002000 /* on-chip RAM block L5 */
/*RAML6 : origin = 0x00E000, length = 0x002000 *//* on-chip RAM block L6 */
/*RAML7 : origin = 0x010000, length = 0x002000 *//* on-chip RAM block L7 */
/*RAML8 : origin = 0x012000, length = 0x002000 *//* on-chip RAM block L8 */
FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA, PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text >> FLASHA | FLASHC PAGE = 0
.cio : > RAML5, PAGE = 1
codestart : > BEGIN, PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAML0 | RAML6L8,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
LOAD_SIZE(_RamfuncsLoadSize),
PAGE = 0
csmpasswds : > CSM_PWL_P0, PAGE = 0
csm_rsvd : > CSM_RSVD, PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0, PAGE = 1
.ebss : > RAML4, PAGE = 1
.esysmem : > RAML5, PAGE = 1
/* Initalized sections to go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA, PAGE = 0
.switch : > FLASHA, PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHA, PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
Cla1Prog : LOAD = FLASHD,
RUN = RAML3,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
LOAD_SIZE(_Cla1funcsLoadSize),
PAGE = 0
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
Cla1DataRam0 : > CLARAM0, PAGE = 1
Cla1DataRam1 : > CLARAM1, PAGE = 1
CLA1mathTables : LOAD = FLASHB,
RUN = CLARAM1,
LOAD_START(_Cla1mathTablesLoadStart),
LOAD_END(_Cla1mathTablesLoadEnd),
RUN_START(_Cla1mathTablesRunStart),
LOAD_SIZE(_Cla1mathTablesLoadSize),
PAGE = 1
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > CLARAM1,
PAGE = 1
/* Allocate FPU math areas: */
FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD
DMARAML5 : > RAML5, PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS, PAGE = 0, TYPE = DSECT
}
////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
I've observed that if Data struct defines a constructor, a compiler warning is thrown:
"warning #10210-D: creating ".esysmem" section with default size of 0x400; use the -heap option to change the default size".
It has no sense for me, it seems that compiler is inferring that heap is needed.
Regards.