This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
I want to convert a variable of type time_t into a timestring in an Interrupt Service Routine like this way:
strftime( PrSealCheckDateStr, 19, ": %d-%m-%Y", localtime( &DateAndTime_t ) );
This works well, if I do this in the main loop. Now my question is:
Can I use the strftime and localtime function in an interrupt Service routine, when I use the functions in the main Loop, too?
Thanks in advance
AWG said:Can I use the strftime and localtime function in an interrupt Service routine, when I use the functions in the main Loop, too?
No. Unfortunately, TI has no solution that supports concurrent multiple activations of localtime.
Thanks and regards,
-George
Hi George,
is there a list of functions that I can call in an interrupt and in the main program at the same time?
Thanks in advance
awg
AWG said:Sometimes I see "Please click Verify Answer on the best reply to your question", but I did not see this button.
That line comes from my signature. You only see it at the end of my posts. Once you click Verify Answer on a post, then that button changes to show Reject Answer. You can click Verify Answer on more than one response in a thread.
AWG said:Is it not enough to click the link in the e-mail: To unsubscribe from only this thread, go here.?
Clicking that link means you no longer receive an e-mail when anyone posts to the associated thread.
Thanks and regards,
-George