This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to update XDS200 firmware



I have a 6657LS eval board, and Code Composer Studio 6.1.1.201508201800.

I'm getting the same error as Don - to run update_xds2xx.bat. But when its done, the swRev is still 1.0.0.2.

  • Rob,

    Interesting, the problem Don was hitting is specific to XDS220. Are you using the XDS200 Mezz card with the 6657 or an external 220? For the 200 Mezz card on the 6657 it should be fine.

    If using an XDS200 try
    xds2xx_conf update xds2xxu 0 sd_xds200_firmware_v1006.bin
    wait till complete and then run
    xds2xx_conf boot xds2xxu 0
    wait until complete and then unplug the usb cable, wait a few seconds and then plug it back in
    then run
    xds2xx_conf get xds2xxu 0

    If using an xds220 connect the usb cable and then try
    xds2xx_conf program xds2xxu 0 xds2xx_xc64_swd.xsvf
    wait till complete
    xds2xx_conf update xds2xxu 0 sd_xds220_firmware_v1006.bin
    wait till complete and then run
    xds2xx_conf boot xds2xxu 0
    wait until complete and then unplug the usb cable, wait a few seconds and then plug it back in
    then run
    xds2xx_conf get xds2xxu 0


    Regards,
    John