When renaming a header file within the CCS IDE, the new header file name is automatically updated throughout the all project. The IDE also updates the new name at all the c files that has #include on that header file. BUT, when it updates the #include to the new name it moves the #inlcude line to the top of the file. This later causes compile cerrors if the order of including was important.
For example, i was using the TivaWare usb_dev_msc example and renamed usb_msc_structs.c/usb_msc_structs.h to usb_msc_sd_structs.c/usb_msc_sd_structs.h.
The list of includes in the original usb_msc_structs.c file is:
#include <stdint.h>
#include <stdbool.h>
#include "driverlib/usb.h"
#include "usblib/usblib.h"
#include "usblib/usb-ids.h"
#include "usblib/device/usbdevice.h"
#include "usblib/device/usbdmsc.h"
#include "usb_msc_structs.h"
#include "usbdsdcard.h"
this is changed after the renaming to:
#include "usb_msc_sd_structs.h"
#include <stdint.h>
#include <stdbool.h>
#include "driverlib/usb.h"
#include "usblib/usblib.h"
#include "usblib/usb-ids.h"
#include "usblib/device/usbdevice.h"
#include "usblib/device/usbdmsc.h"
#include "usbdsdcard.h"
When compiling the project with this new order of include list, usb_msc_sd_struct.h gets compile error because it uses definitions found in file usbdmsc.h which is now included later.
Note: i also noticed that this happens only if you change the c file name first. if you change the h file name first and then the c file name the new name is updated correctly without moving the #include line to the top of the file.
I am using CCS Version: 6.1.1.00022.
Thanks,
Timor