This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
we are running the following filter function on a F2833x Delfino:
static inline FLOAT32 filter3rdOrder(FilterStruct* FilterToCalc)
{
FilterToCalc->fl32out =
FilterToCalc->fl32b0 * FilterToCalc->fl32in
+ FilterToCalc->fl32b1 * FilterToCalc->fl32in_k1
+ FilterToCalc->fl32b2 * FilterToCalc->fl32in_k2
+ FilterToCalc->fl32b3 * FilterToCalc->fl32in_k3
- FilterToCalc->fl32a1 * FilterToCalc->fl32out_k1
- FilterToCalc->fl32a2 * FilterToCalc->fl32out_k2
- FilterToCalc->fl32a3 * FilterToCalc->fl32out_k3;
//Save outputs
FilterToCalc->fl32in_k3 = FilterToCalc->fl32in_k2;
FilterToCalc->fl32in_k2 = FilterToCalc->fl32in_k1;
FilterToCalc->fl32in_k1 = FilterToCalc->fl32in;
FilterToCalc->fl32out_k3 = FilterToCalc->fl32out_k2;
FilterToCalc->fl32out_k2 = FilterToCalc->fl32out_k1;
FilterToCalc->fl32out_k1 = FilterToCalc->fl32out;
return FilterToCalc->fl32out;
}
This functions uses the data structure:
typedef struct
{
FLOAT32 fl32in_k1; // 0x00
FLOAT32 fl32in_k2; // 0x02
FLOAT32 fl32in_k3; // 0x04
FLOAT32 fl32in_k4; // 0x06
FLOAT32 fl32in; // 0x08
FLOAT32 fl32out_k1; // 0x0a
FLOAT32 fl32out_k2; // 0x0c
FLOAT32 fl32out_k3; // 0x0e
FLOAT32 fl32out_k4; // 0x10
FLOAT32 fl32out; // 0x12
FLOAT32 fl32a0;
FLOAT32 fl32a1;
FLOAT32 fl32a2;
FLOAT32 fl32a3;
FLOAT32 fl32a4;
FLOAT32 fl32b0;
FLOAT32 fl32b1;
FLOAT32 fl32b2;
FLOAT32 fl32b3;
FLOAT32 fl32b4;
} FilterStruct;
We do apply Compiler optimization:
--opt_level=2
--opt_for_speed
When we run the filter function with cgt 6.1.6 correct and complete code is generated.
However, when using cgt 6.4.9 (or cgt 15.12.0) compiled code (checked by disassembling the obj or out file) for C instruction "FilterToCalc->fl32out_k2 = FilterToCalc->fl32out_k1;" is missing.
When we run the filter function as non-inlined function correct and complete code is generated even with cgt 6.4.9.
Is this known and expected behavior?
Thx and regards,
Dieter
I cannot reproduce this result. The difference is probably due to other code that is not shown.
Please preprocess the source file with the problem call to filter3rdOrder, and attach it to your next post. Also show the build options exactly as the compiler sees them.
Thanks and regards,
-George
Hello Dieter,
Is FilterToCalc->fl32out_k2 used anywhere in the code? It probably optimized it out because FilterToCalc->fl32out_k2 was not used anywhere else in the code.
Change the function to static inline FLOAT32 filter3rdOrder(volatile FilterStruct * FilterToCalc); and pass it a pomter to a volatile FilterStruct.
Stephen
Dieter Massa said:For providing more code I would need a direct contact.
You can send the code to me privately. Let your mouse float over my forum avatar or user name. A window pops up with a buttons in it. Click on Send a Private Message. A message compose interface comes up. Use the paper clip icon to attach the file.
Thanks and regards,
-George
Thank you for submitting a test case. I can reproduce the problem with the missing assignment to some structure members. I filed SDSCM00052737 in the SDOWP system to have this investigated. You are welcome to follow it with the SDOWP link below in my signature.
Thanks and regards,
-George
Meanwhile I did some deeper investigation and I found the missing instruction:
MOVD32 is used to read the old values of fl32out_k1 and fl32in_k1
According to SPRUE02B assembler instruction "MOVD32 RaH, mem32" operations are:
RaH = [mem32]
[mem32 + 2] = [mem32]
The problem lies deeper:
Compiler version 6.4.9 generates the following code for reading fl32out_k2 and fl32out_k1
0000032f e318 MOV32 R4H, @0xc
00000330 040c
00000331 e223 MOVD32 R3H, @0xa
00000332 030a
What we finally see is that both, fl32out_k2 and fl32out_k3 receive the old value of fl32out_k1.
This can only happen if R4H receives the new value of fl32out_k2 (the value after the MOVD32 partial operation [mem32 + 2] = [mem32] had finished).
Code we generate with cgt 6.1.6 does not contain MOVD32 instructions.
fl32in_k2 and fl32in_k3 are handled correctly. In this case there are a couple of other instructions between reading fl32in_k2 ("MOVL ACC, @0x2") and reading fl32in_k1 and moving fl32in_k1 to fl32in_k2 ("MOVD32 R5H, @0x0").
So, this looks like a pipeline error.
Dieter
Yes, the compiler is generating an MOVD32 instruction, which is why you don't see an explicit write to fl32out_k2, and this is OK.
I cannot reproduce the error. I cannot find any problem with the generated assembly code, and the code executes correctly on an actual TMS320F28377D device.
I am able to reproduce code which has the instructions "MOV32 R3H,@_stFilter_1+12 || ADDF32 R0H,R0H,R3H" and "MOVD32 R2H,@_stFilter_1+10" back-to-back, but I can't quite reproduce exactly the code sequence you are seeing. We need a test case which demonstrates the error. It would help to see the complete generated assembly code for function CtrlFunc.
We have reproduced the problem also on a F28377D microcontroller.
Here is the complete object file disassembly for the simplyfied code
extern FilterStruct stFilter_1; interrupt void CtrlFunc(void) { filter3rdOrder(&stFilter_1); }
.sect ".text:retain"
000000: _CtrlFunc:
000000: .text:retain:
00000000 761b ASP
00000001 fff0 PUSH RB
00000002 abbd MOVL *SP++, XT
00000003 a0bd MOVL *SP++, XAR5
00000004 c2bd MOVL *SP++, XAR6
00000005 c3bd MOVL *SP++, XAR7
00000006 e200 MOV32 *SP++, STF
00000007 00bd
00000008 e203 MOV32 *SP++, R0H
00000009 00bd
0000000a e203 MOV32 *SP++, R1H
0000000b 01bd
0000000c e203 MOV32 *SP++, R2H
0000000d 02bd
0000000e e203 MOV32 *SP++, R3H
0000000f 03bd
00000010 e203 MOV32 *SP++, R4H
00000011 04bd
00000012 e203 MOV32 *SP++, R5H
00000013 05bd
00000014 e203 MOV32 *SP++, R6H
00000015 06bd
00000016 e203 MOV32 *SP++, R7H
00000017 07bd
00000018 e630 SETFLG RNDF32=1,RNDF64=1
00000019 0600
0000001a 2942 CLRC OVM|PAGE0
0000001b 5616 CLRC AMODE
0000001c 761f MOVW DP, #0x0
0000001d 0000
0000001e 0602 MOVL ACC, @0x2
0000001f e2af MOV32 R4H, @0x8, UNCF
00000020 0408
00000021 e2af MOV32 R0H, @0x1e, UNCF
00000022 001e
00000023 e2af MOV32 R1H, @0x20, UNCF
00000024 0120
00000025 bda9 MOV32 R6H, ACC
00000026 0f2a
00000027 e223 MOVD32 R5H, @0x0
00000028 0500
00000029 e301 MPYF32 R0H, R4H, R0H
|| MOV32 R3H, @0x22
0000002a 0322
0000002b e303 MPYF32 R2H, R5H, R1H
|| MOV32 R7H, @0x4
0000002c 5704
0000002d e2af MOV32 R1H, @0x24, UNCF
0000002e 0124
0000002f e741 MPYF32 R3H, R6H, R3H
|| ADDF32 R0H, R0H, R2H
00000030 00f3
00000031 e2af MOV32 R6H, @0x16, UNCF
00000032 0616
00000033 e316 ADDF32 R0H, R0H, R3H
|| MOV32 R3H, @0xc
00000034 030c
00000035 e223 MOVD32 R2H, @0xa
00000036 020a
00000037 e700 MPYF32 R6H, R2H, R6H
00000038 0196
00000039 7700 NOP
0000003a 7700 NOP
0000003b e700 MPYF32 R1H, R7H, R1H
0000003c 0079
0000003d bfa7 MOV32 XAR7, R6H
0000003e 0f2a
0000003f e710 ADDF32 R0H, R0H, R1H
00000040 0040
00000041 bda7 MOV32 R1H, XAR7
00000042 0f16
00000043 7700 NOP
00000044 7700 NOP
00000045 7700 NOP
00000046 c40e MOVL XAR6, @0xe
00000047 e720 SUBF32 R1H, R0H, R1H
00000048 0041
00000049 bda6 MOV32 R0H, XAR6
0000004a 0f12
0000004b 7700 NOP
0000004c e2af MOV32 R7H, @0x18, UNCF
0000004d 0718
0000004e e00e MPYF32 R7H, R3H, R7H
|| MOV32 @0x0, R4H
0000004f fc00
00000050 e2af MOV32 R6H, @0x1a, UNCF
00000051 061a
00000052 e753 MPYF32 R0H, R0H, R6H
|| SUBF32 R1H, R1H, R7H
00000053 9380
00000054 1e04 MOVL @0x4, ACC
00000055 e020 SUBF32 R0H, R1H, R0H
|| MOV32 @0xe, R3H
00000056 430e
00000057 e2af MOV32 R7H, *--SP, UNCF
00000058 07be
00000059 e203 MOV32 @0x12, R0H
0000005a 0012
0000005b e203 MOV32 @0xa, R0H
0000005c 000a
0000005d e2af MOV32 R6H, *--SP, UNCF
0000005e 06be
0000005f e2af MOV32 R5H, *--SP, UNCF
00000060 05be
00000061 e2af MOV32 R4H, *--SP, UNCF
00000062 04be
00000063 e2af MOV32 R3H, *--SP, UNCF
00000064 03be
00000065 e2af MOV32 R2H, *--SP, UNCF
00000066 02be
00000067 e2af MOV32 R1H, *--SP, UNCF
00000068 01be
00000069 e2af MOV32 R0H, *--SP, UNCF
0000006a 00be
0000006b e280 MOV32 STF, *--SP
0000006c 00be
0000006d c5be MOVL XAR7, *--SP
0000006e c4be MOVL XAR6, *--SP
0000006f 83be MOVL XAR5, *--SP
00000070 87be MOVL XT, *--SP
00000071 fff1 POP RB
00000072 7617 NASP
00000073 7602 IRET
This was generated with cl2000 commandline Options:
--keep_asm --quiet --asm_listing --c_src_interlist --optimizer_interlist --large_memory_model --silicon_version=28 --float_support=fpu32 --unified_memory --symdebug:dwarf --opt_level=2 --opt_for_speed
and with compiler:
TMS320C2000 C/C++ Compiler v6.4.9
So far we have always observed this problem.
I.o.w.: There were no situations when the intended operation
FilterToCalc->fl32out_k3 = FilterToCalc->fl32out_k2;
was executed.
Dieter
I think that the disassembly fragment you're showing as the location of the bug is from an entirely different function. I cannot find any sequence of instructions resembling that fragment in the disassembly for _CtrlFunc. Are you absolutely sure that this code is from function _CtrlFunc?
As evidence of my claim: