I am running on a Win 10 system. When I try to edit a file, I find that after typing in a few words or lines, the keyboard entry freezes for a few seconds (<5-10). Sometimes, it seems that my keystrokes have been buffered and they then appear. Other times I'm finding that some of the keystrokes get missed. There have also been times when a keystroke happens multiple times (e.g. thissssssssssssssssssssssss)
This makes program entry difficult.
I am also at a point where my project will not rebuild with my edits - I must issues a Project>Clean command for my code with the "Rebuild after Clean" button pressed so that the clean occurs and then the rebuild happens. This appears to be a carryover of an issue that was reported back with v4. I would think it would be fixed by now.
My project is built up from an empty project example from the RTOS section. I'm developing for a CC1310
Rachel