I have a problem that i cant debug Hello.c in CCSv5
My board is EVMK2H and target configuration is TCI6636K2H.ccxml
MCSDK version is 3_00_03_15
I install many times and try 3_00_03_15 and 3_01_04_07 version.
Besides , i also try to install in windows and linux(Ubuntu 14.04),but both results are the same
I show my console and GEL Output
console :
C66xx_0: GEL Output:
Connecting Target...
C66xx_0: GEL Output: TCI6638K2K GEL file Ver is 1.4
C66xx_0: GEL Output: Detected PLL bypass disabled: SECCTL[BYPASS] = 0x00000000
C66xx_0: GEL Output: (3a) PLLCTL = 0x00000040
C66xx_0: GEL Output: (3b) PLLCTL = 0x00000040
C66xx_0: GEL Output: (3c) Delay...
C66xx_0: GEL Output: (4)PLLM[PLLM] = 0x0000000F
C66xx_0: GEL Output: MAINPLLCTL0 = 0x07000000
C66xx_0: GEL Output: (5) MAINPLLCTL0 = 0x07000000
C66xx_0: GEL Output: (5) MAINPLLCTL1 = 0x00000040
C66xx_0: GEL Output: (6) MAINPLLCTL0 = 0x07000000
C66xx_0: GEL Output: (7) SECCTL = 0x00090000
C66xx_0: GEL Output: (8a) Delay...
C66xx_0: GEL Output: PLL1_DIV3 = 0x00008002
C66xx_0: GEL Output: PLL1_DIV4 = 0x00008004
C66xx_0: GEL Output: PLL1_DIV7 = 0x00000000
C66xx_0: GEL Output: (8d/e) Delay...
C66xx_0: GEL Output: (10) Delay...
C66xx_0: GEL Output: (12) Delay...
C66xx_0: GEL Output: (13) SECCTL = 0x00090000
C66xx_0: GEL Output: (Delay...
C66xx_0: GEL Output: (Delay...
C66xx_0: GEL Output: (14) PLLCTL = 0x00000041
C66xx_0: GEL Output: PLL has been configured (CLKIN * PLLM / PLLD / PLLOD = PLLOUT):
C66xx_0: GEL Output: PLL has been configured (122.88 MHz * 16 / 1 / 2 = 983.04 MHz)
C66xx_0: GEL Output: Power on all PSC modules and DSP domains...
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=2, md=9!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=17, md=25!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=17, md=26!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=18, md=27!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=19, md=28!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=19, md=29!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=20, md=30!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=20, md=31!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=20, md=32!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=20, md=33!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=21, md=34!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=22, md=35!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=22, md=36!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=23, md=37!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=23, md=38!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=24, md=39!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=24, md=40!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=24, md=41!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=24, md=42!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=25, md=43!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=25, md=44!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=25, md=45!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=25, md=46!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=26, md=47!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=27, md=48!
C66xx_0: GEL Output: Power on all PSC modules and DSP domains... Done.
C66xx_0: GEL Output: WARNING: SYSCLK is the input to the PA PLL.
C66xx_0: GEL Output: Completed PA PLL Setup
C66xx_0: GEL Output: PAPLLCTL0 - before: 0x0x07080400 after: 0x0x07080400
C66xx_0: GEL Output: PAPLLCTL1 - before: 0x0x00002040 after: 0x0x00002040
C66xx_0: GEL Output: DDR begin
C66xx_0: GEL Output: XMC setup complete.
C66xx_0: GEL Output: DDR3 PLL (PLL2) Setup ...
C66xx_0: GEL Output: DDR3 PLL Setup complete, DDR3A clock now running at 666 MHz.
C66xx_0: GEL Output: DDR3A initialization complete
C66xx_0: GEL Output: DDR3 PLL Setup ...
C66xx_0: GEL Output: DDR3 PLL Setup complete, DDR3B clock now running at 800MHz.
C66xx_0: GEL Output: DDR3B initialization complete
C66xx_0: GEL Output: DDR done
C66xx_0: Trouble Writing Memory Block at 0xa020 on Page 0 of Length 0x13e: (Error -1190 @ 0x20) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.232.0)
C66xx_0: GEL: File:
Can someone tell a little bit how to solve this bug ? Thanks