Part Number: TMS320C5545
Tool/software: Code Composer Studio
After debug, I always get "
C55xx: Trouble Writing Memory Block at 0x10000 on Page 0 of Length 0x7ff0: (Error -1146 @ 0x10000) Data scanned out of device is corrupt and not valid. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.48.0)
C55xx: File Loader: Verification failed: Target failed to write 0x010000@PROGRAM
C55xx: GEL: File: C:\Users\smk-pc\workspace_v7\CSL_I2S_AudioCodec_DMA\Debug\CSL_I2S_AudioCodec_DMA.out: Load failed.
"
sometimes " Trouble Reading"
How can I solve this?
I'm using c5545 dsp
and I'm testing the example "CLS_I2S_DMA_MultipleInstanceExample_out"
and I modified some code
Please Answer me
thx