This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Why CCS shows the Endianness of SM470R1B1M as LE (little endian)

I am using the BH-USB560-M emulator and CCS6.1.2 with target configuration eZTMS470R1A256 (that is only ARM7 device shown in the CCS target configuration selection) for my device SM470R1B1M (I have specifically changed the endianness as BIG during target configuration setup).

But, after connect CCS to the ARM7 processor, the CCS shows - "Evaluation License, ARM, LE, SPV" at the lower-right cover of CCS window.  The "LE" means Little Endian, I believe. Why? Since the SM470R1B1M is BIG Endian device.
 

Regards!
Wen