This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[C28x] Intrinsics - difference between __byte and __mov_byte



Codegen Gurus,

First question:

  • The prototype for __byte in the compiler guide says: int &__byte(int *array, unsigned int byte_index);
  • The '&' seems to be a typo.  Is that correct?

2nd question:

I've been trying to work out the difference between __byte and __mov_byte

Seems

  • __byte can do either a read from or a write into a byte array. 
  • __mov_byte can only do a read from a byte array

But I'm not clear why one would use __move_byte over just __byte to perform the read.    In the few experiments that I tried these two seem generate the same assembly code and are equiv. operations:

  • val = __byte(Array,index);
  • val = __mov_byte(Array,index);

Is there a difference I've missed?

-Lori

  • Lori Heustess said:

    First question:

    • The prototype for __byte in the compiler guide says: int &__byte(int *array, unsigned int byte_index);
    • The '&' seems to be a typo.  Is that correct?

    It's not a typo, the __byte intrinsic returns a C++-style reference, even in C mode.

    Lori Heustess said:

    I've been trying to work out the difference between __byte and __mov_byte

    __byte can be used on the left-hand side to set values.  This is the reason it needs to return a reference.

    #include <stdio.h>

    int array[3] = { 0xaaaa, 0xbbbb, 0xcccc };

    void main()
    {
    int i;

    __byte(array, 0) = 0;

    for (i=0;i<3;i++)
    printf("%x\n", array[i]);

    for (i=0;i<6;i++)
    printf("%x\n", __mov_byte(array, i));
    }
  • Archaeologist said:
    It's not a typo, the __byte intrinsic returns a C++-style reference, even in C mode.

    Thanks, Brett  - I suspected a reference, but my C++ fu is currently weak.

    Archaeologist said:
    __byte can be used on the left-hand side to set values.  This is the reason it needs to return a reference.

    I'm still not sure I quite understand.  I see the flexibility of __byte.  Why would one use __mov_byte instead?  It seems to be not as useful?

    -Lori

     

  • __mov_byte is much older, and was implemented before the compiler could support an intrinsic that returns a reference.  To maintain backward compatibility, __mov_byte was left as-is, and a new intrinsic (__byte) was added which returns the reference.  You are right, there's nothing you can do with __mov_byte that you can't do with __byte.

  • Great, thanks Brett -

    I've written this up into a wiki article for folks future reference.

    http://processors.wiki.ti.com/index.php/Byte_Accesses_with_the_C28x_CPU

    -Lori