This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv6 Can't find a source file at "/home/test/vision_sdk/example/tda2xx/src/alg_plugins/surroundview/synthesisLink_priv.h"

Host OS : Windows 10

Build Server OS : Ubuntu 14.04

CCS Version : CCS v6.1.1.00022 for windows

Target Board : TDA2x EVM

I'm training TDA2x EVM with VisionSDK v2.7.

Source code is placed in my Ubuntu server and compiled from there.

CCS is installed my Windows PC 

Ubuntu server is connected via network drive Z:\

In debugging on CCS, I see a message "Can't find a source file at /home/test/visionSDK_v2.7/vision_sdk/example/tda2xx/src/alg_plugins/surroundview/systhesisLink_priv.h

Locate the file or edit the source lookup path to include its location" when I suspend DSP 1.

I know the path "/home/test" is "Z:\" and I want to remap the path 

How can I do this on CCS v6 ? 

Best regards

Jeon.