This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5.5 BlackHawk XDS100v2 TMS570LS1227

Hi,

 

I am using CCS5.5 and a BlackHawk XDS100v2 USB connected to an in-house design using the TMS570LS1227PGE (Rev C) and the Ti 20pin interface.

 

The code i wish to program into the device falls over with the message below:

 

CortexR4: Flash Programmer: Error erasing Bank 0, Sector 0. Operation Cancelled.

CortexR4: Unable to terminate memory download: (Error -1003 @ 0x2BC5) Internal error: Invalid parameter passed to function. Restart the application. If error persists, please report the error. (Emulation package 5.1.232.0)

CortexR4: GEL: File: C:\Users\COL117\workspace_v5_5\Gate_Drive_Test\Debug\Gate_Drive_Test.out: Load failed.

Looking at the folder, the .out file is present with a recent build timestamp so the message is a little confusing.

 

The Test Connection feature in the tool shows that the JTAG connection passes all tests so I know that the MCU and JTAG emulator are communicating.

The electrical connectivity is the same as a development card which does manage to program but the only difference is the silicon revision (Rev B)

Is there a configuration setting I am missing?

PS. as the error is persisting I am reporting it as per the instruction :)