I thought I had installed the C/C++ PRU compiler via the App center. However when I start to create a project under a Beaglebone black target, select the PRU tab, there is no compiler displayed. The compilers are displayed for the Cortex tabs.
I installed the C/C++ compiler as root. When I look at the App center it is reporting that the compiler is up to date. I have tried a search in the sdk I have installed, and in the ti folder for the binary but it can't find it.
Am I missing a path somewhere ? Does anyone know where the compiler should be installed so I can link it manually ?
Thanks,
Paul