This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi John,
Thanks for looking into it. I use another G2 board from 2013 and run it on windows 10 cloud CCS. It works in that configuration. I will bring this board home and try it again on mac. The G2 I tried it earlier is from 2011 or 2012.
best,
frank
Tried two G2 boards on mac. No, it won't run. The same rf2500 failure. In fact, the debug button is greyed out.
To summarize what I found:
Cloud CCS works for my teaching need (entry level programming) on Windows 10 PC. 430G2, 430F5529 and 432P401 works.
But, cloud CCS on Mac works on 430F5529 and 432P401, but NOT 430G2 (neither run nor debug). BTW, for our teaching purpose, debug is the only mode we do.
Given today's student machines (mac/pc/chromebook), using cloud CCS is probably the way to proceed. hmmm, maybe time to switch board...
Frank,
On mac, CCS Cloud uses mspdebug to flash G2 devices. I believe you have another usb driver that it taking control of the G2 usb connection and making it impossible for mspdebug to access it. You can workaround this by installing a codeless kernel extension that indicates it supports the G2, but does nothing, leaving it available for mspdebug to use. You can download it here.
I've attached a pre-built version to this thread in case you have issues with the xcode project. However, you'll still have to follow the instructions at the link to install it.
Darian
Thanks Darian. If usb is taken over by another device, why would it work with F5529?
In any event, I will switch my teaching board to F5529 for the next semester. The good thing is that there are only minor differences for my use. Green LED move from P1.6 to P4.1, button is moved too.
The 5529 uses the msp430.dll to flash/debug, and not mspdebug, and thus works completely differently. Also, if you switch to the 5529, you'll have debug capabilities (breakpoints, step, expression evaluate etc), whereas with the 2553 you'll only be able to flash your code and run it (at least on mac).
Darian