Hi,
I am getting a Compiler Aborting message when it is trying to compile a right shift of a uint64_t.
HWREG_BP(base + CAN_O_IF1DATB) = (uint32_t)(dataValue >> 32UL);
Compiler Message:
C:/ti/c2000/C2000Ware_0_04_00_06/libraries/soprano_60730_class_c/f2837xd/source/stl_can.c, line 417:
INTERNAL ERROR: no match for ASG
This may be a serious problem. Please contact customer support with a
description of this problem and a sample of the source files that caused this
INTERNAL ERROR message to appear.
Cannot continue compilation - ABORTING!
gmake: *** [stl_can.obj] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
Regards,
sal