This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377D - CPU1 and CPU2 debug as a group

Other Parts Discussed in Thread: CONTROLSUITE

I am having some inconsistent behavior when grouping CPU1 and CPU2 in the debug environment. The intent is to suspend and resume execution as a group, rather than individually. The problem is that CPU2 does not properly execute the code. Please note that if I resume execution individually, both CPU's operate perfectly - the issue only happens when I group them. My suspicion is that CPU2 is taking off before the JTAG can take control of it, causing the code to abort. Here is a snapshot of my debug window:

Some details:

- Using the F28377D control card on docking station

- controlSUITE version 3.4.3, device support v210

- CCS version 6.2.0.00048 

- Blinky project running on RTOS - both cores have similar code. I confirm proper execution by observing the LED's.

- the same problem is observed with the customer's setup.

My question is: how can we enable proper execution when the CPU's are grouped. If not possible, do we have any workaround?

Thank you!