Part Number: TMDSEZ28335
Tool/software: Code Composer Studio
I am using it with Windows 8.1 pro with media edition and TI kit eZDSPtms320F28335. I installed code composer studio 6.0.1 and it is having full license. I am using Signam Jtagjet C200 F-ISO. I downloaded JTAG driver v6.0.0 from web for and installed. I tested the connection with EMUdiag. It is working fine with no error. When I am tring to connect with code composer, the following error appears:
Error: ret jsc_connect
Error 0x80000240/-171 Fatal Error during: Initialization, OCS,
"Test Connection" button in code composer remain greyed colour.