Part Number: TDA2EVM5777
Tool/software: Code Composer Studio
Dear ,
We got TDA2x evm board from Spectrum Digital.
Now we want to debug code every cores by Emulator(SW:CCS6.1.3,emulator:SEED-XDS560v2 ).
Some questions about connection of ccs6.1.3 by .gel files on TDA2x platform as follows:
1There are 14 CPU cores on CCS debug GUI after launching CCS .ccxml configuration.
Firstly I connected Cortex-A15_0 core, but there some error information as follows:
could you tell me which factors cause this phenomenon?
In addition,I connected the others core in following sequence after connecting A15_0 with some error information mentioned above;
A15_1,ARM_ICONT1, ARM_ICONT2, M4_IPU1_C0, M4_IPU1_C1,
M4_IPU2_C0, M4_IPU2_C1,C66xx_DSP1, C66xx_DSP2,ARP32_EVE_1,
ARP32_EVE_2, ARP32_EVE_3, ARP32_EVE_4,
Except DSP2 and four EVEs cannot be connected,the other cores can be connected normally.
DSP2: information for disconnecting
Error connecting to the target:
(Error -1180 @ 0x0)
Device is held in reset. Take the device out of reset, and retry the operation.
(Emulation package 6.0.222.0)
Four EVEs: information for disconnecting:
Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 6.0.222.0)
could you give me some suggestions for all cores' connection?
Thanks a lot!
BRS,
Meng