This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi E2E,
I have a customer with some questions regarding CCS. Their IT department is setting up a new license server so that their existing license managers can be moved to that server. They are using CCSv5.2.1.
1. What is the latest version of FlexNet license server tool that can support the CCS version 5.2.1? Can FlexNet v 11.13.1 support CCS v 5.2.1? They need this information as they need to make sure that the Flexnet version is also compatible with other license tools that will be run on the same server.
2. Is the license manager version compatible with Windows server 2012 R2 64 bit O/S? If yes, then what version?
3. Are there any special hardware requirements for the license manager to run in terms of CPU, RAM, Storage requirements etc.?
Thanks,
-Sam