This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: How to flash .OUT file to 28335 with CCSV4 (4.2)

Part Number: TMS320F28335

Tool/software: Code Composer Studio

Hi,

I m using experimenter kit for TMS320F28335 and I m using MATLAB/Simulink for the software. The matlab generates .out file and I can debug this .out file using CCSv4. How can I flash this .out file so that the TMS320F28335 can start the code whenever it is powered on?

  • Hi Murat,

    Check your simulink configuration for whether the generated code is RAM or FLASH based. The generated code has to be Flash based for standalone operation.

    Regards,
    Gautam
  • Where is the setting for Flash or Ram based generation? What is needed in CCSV4 and experimenter kit switches to flashing the code? If it helps, I can take snapshots of smulink setttings and share here.

    Regards,

    Murat