This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
I m using experimenter kit for TMS320F28335 and I m using MATLAB/Simulink for the software. The matlab generates .out file and I can debug this .out file using CCSv4. How can I flash this .out file so that the TMS320F28335 can start the code whenever it is powered on?
Where can I generate flash based simulink code? What are settings in configuration parameters? What should be the system target file to generate flash based code?
Best regards,
Murat Kayhan
I read the document but I forgot to say I'm using Matlab2011b and the hardware implementation pane does not have Flash loader property.
I'm using Matlab 2011b and in code generation pane I choose idelink_ert for system target file. I do not have any problem to generate .out file but I only use this out file for debugging. I could not achieve TMS320F28335 working from flash memory. I'm using experimenter kit and I set the switch settings for boot from flash but still not working. I'm sharing my Matlab Code generation screen.