This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: CCS/TMS320F28335: How to flash .OUT file to 28335 with CCSV4

Part Number: TMS320F28335

Tool/software: Code Composer Studio

Hi,

I m using experimenter kit for TMS320F28335 and I m using MATLAB/Simulink for the software. The matlab generates .out file and I can debug this .out file using CCSv4. How can I flash this .out file so that the TMS320F28335 can start the code whenever it is powered on?

Where can I generate flash based simulink code? What are settings in configuration parameters? What should be the system target file to generate flash based code?

Best regards,

Murat Kayhan