This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/RM48L952: CCSv7 forbids to debug with Segger J-Link because of endianess

Part Number: RM48L952
Other Parts Discussed in Thread: SEGGER,

Tool/software: Code Composer Studio

Hi,

    I'm trying to debug an Hercules RM48 software using CCSv7 and Segger J-Link.

    Unfortunately, the debug is aborted prior to flashing the device, with the following error:

    "CortexR4: GEL: File: C:\\workspace_v7\Test\Debug\Test.out Does not match the target endianness, not loaded. Check project build options and target configuration file (ccxml)."

    The target configuration file is already configured for little endian, but the error persists.

    What can I do to debug the RM48 software through J-Link USB in CCSv7?

     Facts:

     - Hercules RM48 ARM Cortex-R4 processor

    - Code Composer Studio version 7.0.0.00043

    - CCS Segger J-Link version 6.10.0.n

    Best regards,

--
    Reggie Vivekananda
    Software Engineer
    ART - Alta Rail Technology
    Visit our website: http://www.alta-rt.com/
    -= Be conscious, print only what is really needed =-