Part Number: CC3200
Tool/software: Code Composer Studio
Hello,
I'm not sure if this is the right place to post this, but I would like to graph variables from my CC3200 in real time and maybe even control some of its outputs. I stumbled across GUI Composer and it seems like what I need. I went to the wiki and it says GUI Composer is not supported for CCS for v6.2 and directed my to the cloud based Gui Composer v2. I tried creating a project (Dashboard version) using this and selecting the CC3200 as my target device and USB as my method of communication and it wanted me to upload a "Target Executable". I have no idea what this is. All it said was this is a .out or .cpp.hex file. I would like to use this GUI composer with an existing CCS v6.2 project I have for the CC3200. Is there documentation on how to do this? I tried looking at all the wiki and help pages I could but the documentation seems lacking. Can anyone help?
Thanks,
John