This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hey guys,
I downloaded the Project 0 demo project from the cloud based compiler. The includes reference a myriad of components that I do not have locally and I was wondering where I might be able to find them so that the project will build. My includes reference the variable ${TI_BLE_SDK_BASE} which evaluates to ${TI_PRODUCTS_DIR}/simplelink/ble_cc26xx_2_01_00_44423_cloud. ${TI_PRODUCTS_DIR} is C:/ti.
I'm missing the ble_cc26xx_2_01_00_44423_cloud folder and all referenced subfolders. Which package might I be missing? I have ble_sdk_2_02_01_18 under simplelink, but no others. I would try changing the reference to be the different version of simplelink and the sdk that I have but I'd still be missing subfolders/subcomponents.
Any pointers would be appreciated.
Thanks!
Seems some of the other imports are not working now. Seems I'm missing buildConfig.opt for the project.
Edit: after locating a version of buildConfig.opt and changing the location of it, I then needed OSAL_ICallBLE.c. Found a version of this and installed it in the proper location. After that I still have some build errors which are below:
<Linking> undefined first referenced symbol in file --------- ---------------- GAPBondMgr_CheckNVLen <whole-program> GAPBondMgr_GetParameter <whole-program> GAPBondMgr_Init <whole-program> GAPBondMgr_LinkEst <whole-program> GAPBondMgr_LinkTerm <whole-program> GAPBondMgr_PasscodeRsp <whole-program> GAPBondMgr_ProcessEvent <whole-program> GAPBondMgr_Register <whole-program> GAPBondMgr_ResolveAddr <whole-program> GAPBondMgr_ServiceChangeInd <whole-program> GAPBondMgr_SetParameter <whole-program> GATTServApp_SendServiceChangedInd <whole-program> >> Compilation failure makefile:187: recipe for target 'ProjectZeroStack_CC2650LAUNCHXL.out' failed error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "ProjectZeroStack_CC2650LAUNCHXL.out" not built gmake: *** [ProjectZeroStack_CC2650LAUNCHXL.out] Error 1 gmake: Target 'all' not remade because of errors. **** Build Finished ****
Don't really know how to fix these errors. I'd appreciate any guidance.
------------------------------------------------------------------------
Importing the project from SimpleLink Academy only got me half a step farther. Now it's causing an error when debugging. It gets to BIOS_Start() then fails out at loader_exit() immediately. Not sure exactly where I might discover the cause of this.