This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
i downloaded ccs4.x for f28035 but i could not use ccs4.x when flash mode.
i wonder that can i use ccs3.x for f28035??
i read that the f28035 can not be programmed by ccs3.x. is it correct?
For 3.x support, make sure you have the latest Service Release (12) and the CSP and Flash plugin for f2803x
Get SR12 from Update Advisor
CSP: http://software-dl.ti.com/dsps/dsps_registered_sw/sdo_ccstudio/CCSv3/CSPS/F2803x_CSP_v3.3.2901.exe
Flash plugin: http://software-dl.ti.com/dsps/dsps_registered_sw/sdo_ccstudio/CCSv3/CSPS/F2803x_CSP_v3.3.2903.exe
Thanks
ki
firstly, thank you for your attention.
but when i want to update latest Service Release (12), the web site wants Service Code from me..
where can i find service code?
CCS3.X cd on my hand, but nothing write on it!!!!
when i bought piccolo mcu control stick, the ccs3.3 cd came with it. but nothing write on it??
Can you check what version of CCS came with your control stick? I need the full version number. You may already have the latest SR.
ali eren said:i downloaded ccs4.x for f28035 but i could not use ccs4.x when flash mode.
2803x is supported in CCS 4 in 4.1.2 and later. Please provide more details as to how it is not working? Does CCS give any error messages? Is it the programming that isn't working or boot to flash?
http://processors.wiki.ti.com/index.php/Development_Tool_Versions_for_C2000_Support
-Lori
the service releases for CCSv3.3 are here
https://www-a.ti.com/downloads/sds_support/CCSv3.3ServiceReleases.htm
In CCSv4, it's a bit confusing (IMO). You don't use the "Flash Plug-in", you just click on the project and set the active build configuration to Flash. Then when you load the program it automatically flashes the device.
version number of my hand is 3.3.81.28.
i dont have any error mesage.
and
which pins must be changed for flash mode(stand alone)? and that pins high or low???
i read that"Stand-alone boot: If an emulation controller is not connected, then the boot ROM will use two GPIO pins to determine how to boot the device. "
my problem is that. when i disconnect the emulator and the hardware start again , the programme doesnt start.