Tool/software: Code Composer Studio
Version: 6.1.3.00034
How to enable full file path to be visible when editing source code in IDE?
I believe that this is a must, especially because the ambiguity caused by the multiple project folder variables that you have in code composer:
ORIGINAL_PROJECT_ROOT
PARENT_LOC
PROJECT_LOC
WORKSPACE_LOC
origin_value In .ccsproject
At least, it would be a normal to introduce 'save as' with the full path! It seems as a basic requirement for any editor.
I already managed to save source file into completely wrong folder, that was used for one of the predecessor projects.
Again, my question is: what to set to see the absolute path of the edited source file?
Sincerely,
Vlad Pavlovic