Part Number: DRA756
Tool/software: Code Composer Studio
Hi,
I'm trying to step through an assembly function running on the Cortex A15_0 core of a DRA75x device. The assembly function is compiled directly from source within my CCS project (not from a library), and I have debug information enabled in the compiler flags. When I step into the assembly function, I see a window displaying the following:
So I lose my call stack, and the debugger can't associate to the source when stepping through the code. I can step through the disassembly, but I would prefer to use the source itself (with comments, declaration aliases, etc.).
I am using the following tools: bios_6_50_01_12, CCSv7.1.0, uia_2_20_00_02, xdctools_3_50_02_20_core, gcc-arm-none-eabi-4_9-2015q3.
GCC compiler settings for the asm file: "-mcpu=cortex-a15 -mtune=cortex-a15 -marm -mfloat-abi=hard -g -gdwarf-3 -gstrict-dwarf -Wall"
Is there something else that I'm missing here?
Thanks,
Stephen