This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm running Code Composer 4.1 with Windows XP. My problem is that when I compress a project folder using the 'Send To' file compression utility any folder starting with a . (.metadata, .launches and .settings) aren't being included in the compressed file. Any ideas on how to get these folders included in the .zip?
This is not a CCS issue but an issue with the default windows zip utility that you are using. It seems to filter out files/folders that start with a period. You can probably change this setting somewhere in windows (I don't know where). I don't use the windows zip utility but instead I use winzip or winrar and both of those have no issue.
Thanks
ki
Thank you for your quick reply.
I only brought this up because I've been zipping folders in this manner for years using various development system and have never had a problem. Part of the problem here is that Code Composer/ Eclipse is using . in front of folder names which is not completely Window's XP friendly. I managed to correctly zip my project folders under Window's XP by using the command line 'compact' command.
Thanks again.
Yes, that is a standard Eclipse thing. Eclipse is cross platform and not just Windows focused. Thanks for the update