Hi,
We are sharing a project through a source control application (Perforce) and to make it portable, each project has its macros.ini file which defines relative paths necessary for it to build (see attached file).
On my computer (Windows 7), when I import a project from the source control application, the macros are correctly assigned in the Preferences -> General -> Workspace -> Linked Resources window. Then, I can correctly build the project.
On my colleague's computer (Windows Vista), when we import the same project, the macros are not assigned in that same window. Moreover, even if I manually create them in that window, they are not reflected in the project. In order to make the project work as expected, I need to go inside the project build options and create the macros there.
Is there something wrong with the way we are proceeding?
Thanks
Franck