Other Parts Discussed in Thread: MSP430-FLASHER
Tool/software: Code Composer Studio
Hi,
While using MSP-FET with Code Composer Studio 6.0.1, it recently asked if some update is required. I was using the interface without the update and without any issue.
Once, by mistake, I pressed the update button. In the process, the MSP-FET has stopped working. The CCS shows "Interface Communication Error" with the MSP-FET.
Using other versions of CCS (ver.7) or uninstalling and re-installing the FET drivers or using on other PCs gives the same error message.
On connecting to USB port, the green LED is lighting up in the FET, but no voltages are coming on the output connector.
I suspect that on pressing "update" option in the CCS, it messed up the firmware in the FET.
Please suggest possible remedies.
Thanks and regards,