Part Number: LAUNCHXL-CC2640R2
Tool/software: Code Composer Studio
Hello,
I would like to add the following variable to the configuration file "app_ble.cfg": "var FatFS = xdc.useModule('ti.mw.fatfs.FatFS');"
When I do it in the SimpleBLEPeripheral of the new SDK 1.4 for the CC2640R2, I get the following error:
"C:/ti/simplelink_cc2640r2_sdk_1_40_00_45/kernel/tirtos/packages/ti/sysbios/knl/Swi.c", line 483: error: identifier "Error_IGNORE" is undefined 1 error detected in the compilation of "C:/ti/simplelink_cc2640r2_sdk_1_40_00_45/kernel/tirtos/packages/ti/sysbios/knl/Swi.c". gmake[1]: *** [rom_sysbios.obj] Error 1 gmake: *** [C:/Users/emocs/workspace_v7/simple7314/simple_peripheral_cc2640r2lp_app/TOOLS/src/sysbios/rom_sysbios.aem3] Error 2 error: xdc.cfg.SourceDir: "C:/ti/xdctools_3_30_06_67_core/packages/xdc/cfg/SourceDir.xs", line 184: xdc.cfg.SourceDir : Build of generated source libraries failed: exit status = 2: js: "C:/ti/xdctools_3_30_06_67_core/packages/xdc/cfg/Main.xs", line 160: Error: Configuration failed! xdctools_3_30_06_67_core\gmake.exe: *** [package/cfg/app_ble_pem3.xdl] Error 1 xdctools_3_30_06_67_core\gmake.exe: *** Deleting file `package/cfg/app_ble_pem3.xdl' xdctools_3_30_06_67_core\gmake.exe: *** [package/cfg/app_ble_pem3.xdl] Deleting file `package/cfg/app_ble_pem3.h' xdctools_3_30_06_67_core\gmake.exe: *** [package/cfg/app_ble_pem3.xdl] Deleting file `package/cfg/app_ble_pem3.c' js: "C:/ti/xdctools_3_30_06_67_core/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted. gmake[1]: *** [build-1287780815-inproc] Error 1 gmake: *** [build-1287780815] Error 2 gmake[1]: Leaving directory 'C:/Users/emocs/workspace_v7/simple7314/simple_peripheral_cc2640r2lp_app/FlashROM_StackLibrary' TOOLS/subdir_rules.mk:9: recipe for target 'build-1287780815' failed gmake: Target 'all' not remade because of errors.
Could you please help me of how I can solve this problem?
Thank you in advance,